1.6.6 SAML10 Xplained Boost Mode Example using T10 Xplained Pro Mutual

Path of the application within the repository is apps/t10_mutualcap_xpro_board/sam_l10_xpro_boost_mode/

To build the application, refer to the following table and open the project using its IDE.

Project NameDescription
sam_l10_xpro_boost_mode\firmware\sam_l10_xpro.XMPLABX Project for SAML10 Xplained Pro Evaluation Kit

Hardware Setup

  • Project uses SAML10 XPlained Pro Evaluation Kit and T10 Xplained Pro Extension Kit
  • Connect EXT3 of T10 Xplained Pro to EXT1 of SAML10 Xplained Pro
  • Connect the Debug USB port on the board to the computer using a micro USB Cable

Running the Application

  1. Open the application project sam_l10_xpro.X in the IDE
  2. Build the project and program the target board
  3. Configure COM Port
    • Select Autoconfigure in Variable Streamers tab
    • Select the correct COM port in source
    • Configuration files are stored as part of the project source files
    • In Auto Configure Options, browse the ../touch/datastreamer/ project folder and click on Select Folder
    • Update the Baud Rate to 115200 in COM Settings
    • Start Streaming for COM data

Detailed procedure can be found in Visualize Touch Data Using MPLAB® Data Visualizer page.