1.3.11 PIC32CM PL10 Water Tolerance Demo Application using QT7 Xplained Pro Self
Path of the application within the repository is apps/qt7_selfcap_xpro_board/pic32_cm_pl10_cnano_water_tolerance/
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description |
|---|---|
| firmware\pic32cm_pl10_qt7.X | MPLABX Project for PIC32CM PL10 Curiosity Nano Evaluation Kit |
Hardware Setup
- Project uses PIC32CM PL10 Curiosity Nano Evaluation Kit and QT7 Xplained Pro Evaluation Kit
- Place the Curiosity Nano Evaluation board on the Curiosity Nano Touch Adaptor
- Connect EXT1 of QT7 Xplained Pro to EXT1 of Curiosity Nano touch Adapter
- Connect the USB port on the board to the computer using a USB-C Cable
Running the Application
- Open the application project pic32cm_pl10_qt7.X in the IDE
-
Build the project and program the target board
-
Configure COM Port
- Select Autoconfigure in Variable Streamers tab
- Select the correct COM port in source
- Configuration files are stored as part of the project source files
- In Auto Configure Options, browse the ../touch/datastreamer/ project folder and click on Select Folder
- Update the Baud Rate to 115200 in COM Settings
- Start Streaming for COM data
Detailed procedure can be found in Visualize Touch Data Using MPLAB® Data Visualizer page.