This chapter describes the operation and the usage of the linker.
The application name of the linker is hlink
. In most
instances it will not be necessary to invoke the linker directly, as the compiler driver, xc8-cc
, will automatically
execute the linker with all the necessary arguments. Using the linker directly is not
simple, and should be attempted only by those with a sound knowledge of the requirements of
the linking process. If psects are not linked correctly, code failure can result.