Convert wide string to an unsigned long long integer value.
Include
<wchar.h>
Prototype
unsoigned long long int wcstoull(const wchar_t * restrict nptr, wchar_t **
restrict endptr, int base);
Arguments
nptr | |
endptr | |
base |
Return Value
The converted value, or 0 if the conversion could not be performed. If the correct value of
the conversion is outside the range of representable values, ULLONG_MAX
is
returned.
Remarks
The wcstoull
function attempts to convert a portion of the wide string
pointed to by nptr
to a unsigned long long int
value.
The initial sequence consists of any white-space wide characters.
The subject sequence represents the integer constant to convert and whose radix is
given by base
.
If the value of base
is zero, the expected form of the subject
sequence is that of an integer constant whose radix is determined by the sequence
itself. For example, a leading 0x
implies a hexadecimal constant; a
leading 0
implies an octal constant. The sequence may be preceded
by a plus or minus sign, but not including an integer suffix.
If the value of base
is between 2 and 36 (inclusive), the expected
form of the subject sequence is a sequence of letters (a
(or
A
) through z
(or Z
) ascribed
the values 10 through 35) and digits representing an integer with the radix
specified by base
. Only letters and digits whose ascribed values
are less than that of base
are permitted. The sequence may be
preceded by a plus or minus sign, but not including an integer suffix. If the value
of base
is 16, the wide characters 0x
or
0X
may prefix the sequence of letters and digits, following the
sign wide character if present.
Conversion stops once an unrecognized wide character is encountered, thus the subject
sequence is defined as the longest subsequence of the input wide string after the
initial sequence and that is of the expected form. A pointer to the position of the
first unrecognizable wide character in the wide string is stored in the object
pointed to by endptr
, provided that endptr
is not
a null pointer.
The final sequence consists of wide characters in the wide string that were
unrecognized in the subject sequence and which will include the terminating null
wide character of the wide string. This sequence of the wide string will be
accessible via the address stored to endptr
, provided
endptr
is not a null pointer.
The value of the macro ERANGE
is stored in errno
if
the correct value of the conversion is outside the range of representable
values.
Example
#include <wchar.h>
int main ()
{
wchar_t ws[] = L"2001 60c0c0 -1101110100110100100000 7000 07000";
wchar_t * pEnd;
unsigned long long int ulli1, ulli2, ulli3, ulli4, ulli5;
ulli1 = wcstoull(ws, &pEnd, 10);
ulli2 = wcstoull(pEnd, &pEnd, 16);
ulli3 = wcstoull(pEnd, &pEnd, 2);
ulli4 = wcstoull(pEnd, &pEnd, 16);
ulli5 = wcstoull(pEnd, NULL, 0);
wprintf(L"The converted string values in decimal are: %llu, %llu, %llu, %llu, and %llu.\n", ulli1, ulli2, ulli3, ulli4, ulli5);
}
Example Output
The converted string values in decimal are: 2001, 6340800, 18446744073705927392, 28672, and 3584.