Moves file pointer to a specific location.
Include
<stdio.h>
Prototype
int fseek(FILE * restrict stream, long offset, int
mode);
Arguments
stream | |
offset | |
mode |
Return Value
Returns 0 if successful; otherwise, returns a non-zero value
and set errno
.
Remarks
mode
can be one of the following tabulated values.
Mode | Description |
---|---|
SEEK_SET |
seeks from the beginning of the file |
SEEK_CUR |
seeks from the current position of the file pointer |
SEEK_END |
seeks from the end of the file |
Example
#include <stdio.h>
int main(void)
{
FILE *myfile;
char s[70];
int y;
myfile = fopen("afile.out", "w+");
if (myfile == NULL)
printf("Cannot open afile.out\n");
else
{
fprintf(myfile, "This is the beginning, this is the middle and this is the end.");
y = fseek(myfile, 0L, SEEK_SET);
if (y)
perror("Fseek failed");
else
{
fgets(s, 22, myfile);
printf("\"%s\"\n\n", s);
}
y = fseek(myfile, 2L, SEEK_CUR);
if (y)
perror("Fseek failed");
else
{
fgets(s, 70, myfile);
printf("\"%s\"\n\n", s);
}
y = fseek(myfile, -16L, SEEK_END);
if (y)
perror("Fseek failed");
else
{
fgets(s, 70, myfile);
printf("\"%s\"\n", s);
}
fclose(myfile);
}
}
Example Output
"This is the beginning"
"this is the middle and this is the end."
"this is the end."
Example Explanation
The file afile.out
is created with the
text, “This is the beginning, this is the middle and this is the end.”
The function fseek
uses an offset of zero
and SEEK_SET
to set the file pointer to the beginning of
the file. fgets
then reads 22 characters which are “This
is the beginning,” and adds a null character to the string.
Next, fseek
uses an offset of two and
SEEK_CURRENT
to set the file pointer to the current
position plus two (skipping the comma and space). fgets
then reads up to the next 70 characters. The first 39 characters are “this
is the middle and this is the end.” It stops when it reads
EOF
and adds a null character to the string.
Finally, fseek
uses an offset of negative
16 characters and SEEK_END
to set the file pointer to 16
characters from the end of the file. fgets
then reads up
to 70 characters. It stops at the EOF
after reading 16
characters “this is the end,” and adds a null character to the string.