Calculates the quotient and remainder of two numbers.
Include
<stdlib.h>
Prototype
div_t div(int numer, int denom);
Arguments
numer | |
denom |
Return Value
Returns the quotient and the remainder.
Remarks
The returned quotient will have the same sign as the numerator divided by the
denominator. The sign for the remainder will be such that the quotient times the
denominator plus the remainder will equal the numerator (quot * denom + rem =
numer
).
If either part of the result cannot be represented, such as when attempting to perform a division by zero, the behavior is undefined. MPLAB XC compiler might raise an exception in such circumstances.
Example
See the notes at the beginning of this chapter or section for
information on using printf()
or scanf()
(and other functions reading and writing the stdin
or
stdout
streams) in the example code.
#include <stdlib.h>
#include <stdio.h>
int main(void)
{
int x, y;
div_t z;
x = 7;
y = 3;
printf("For div(%d, %d)\n", x, y);
z = div(x, y);
printf("The quotient is %d and the remainder is %d\n\n", z.quot, z.rem);
x = 7;
y = -3;
printf("For div(%d, %d)\n", x, y);
z = div(x, y);
printf("The quotient is %d and the remainder is %d\n\n", z.quot, z.rem);
x = -5;
y = 3;
printf("For div(%d, %d)\n", x, y);
z = div(x, y);
printf("The quotient is %d and the remainder is %d\n\n", z.quot, z.rem);
x = 7;
y = 7;
printf("For div(%d, %d)\n", x, y);
z = div(x, y);
printf("The quotient is %d and the remainder is %d\n\n", z.quot, z.rem);
}
Example Output
For div(7, 3)
The quotient is 2 and the remainder is 1
For div(7, -3)
The quotient is -2 and the remainder is 1
For div(-5, 3)
The quotient is -1 and the remainder is -2
For div(7, 7)
The quotient is 1 and the remainder is 0