Copies n characters of the source buffer into the destination buffer, even if the regions overlap.
Include
<string.h>
Prototype
void *memmove(void *s1, const void *s2, size_t
n);
Arguments
s1 | |
s2 | |
n |
Return Value
Returns a pointer to the destination buffer.
Remarks
If the buffers overlap, the effect is as if the characters are read first
from s2
, then written to s1
, so the buffer is not
corrupted.
Example
See the notes at the beginning of this chapter or section for
information on using printf()
or scanf()
(and other functions reading and writing the stdin
or
stdout
streams) in the example code.
#include <string.h>
#include <stdio.h>
int main(void)
{
char buf1[50] = "When time marches on";
char buf2[50] = "Where is the time?";
char buf3[50] = "Why?";
printf("buf1 : %s\n", buf1);
printf("buf2 : %s\n", buf2);
printf("buf3 : %s\n\n", buf3);
memmove(buf1, buf2, 6);
printf("buf1 after memmove of 6 chars of "
"buf2: \n\t%s\n", buf1);
printf("\n");
memmove(buf1, buf3, 5);
printf("buf1 after memmove of 5 chars of "
"buf3: \n\t%s\n", buf1);
}
Example Output
buf1 : When time marches on
buf2 : Where is the time?
buf3 : Why?
buf1 after memmove of 6 chars of buf2:
Where ime marches on
buf1 after memmove of 5 chars of buf3:
Why?