Get a character from stdin
.
Include
<stdio.h>
Prototype
int getchar(void);
Return Value
Returns the character read or EOF
if a read error occurs or end-of-file
is reached.
Remarks
This function is equivalent to fgetc
with the argument
stdin
.
When building with the MPLAB XC8 compiler for PIC MCUs, the getchar()
function relies on the getch()
function being properly defined to
obtain input from the required peripheral or location. Reading will not work as expected
until the getch()
stub (found in the
pic/sources/c99/common/getch.c of your compiler distribution)
is completed. See Example code for 8-bit PIC MCUs
for information on defining getch()
so that text can be read from a
file in the MPLAB X IDE simulator.
Example
#include <stdio.h>
int main(void)
{
char y;
y = getchar();
printf("%c|", y);
y = getchar();
printf("%c|", y);
y = getchar();
printf("%c|", y);
y = getchar();
printf("%c|", y);
y = getchar();
printf("%c|", y);
}
Example Input
Contents of UartIn.txt
(used as stdin
input for
simulator):
"Short
Longer string"
Example Output
S|h|o|r|t|