Calculates the arc hyperbolic sine function of a double precision floating-point value.
Include
<math.h>
Prototype
double asinh(double x);
Argument
x |
Return Value
Returns the arc hyperbolic sine of x
.
Example
See the notes at the beginning of this chapter or section for
information on using printf()
or scanf()
(and other functions reading and writing the stdin
or
stdout
streams) in the example code.
#include <math.h>
#include <stdio.h>
#include <errno.h>
int main(void)
{
double x, y;
errno = 0;
x = -1.0;
y = asinh(x);
if (errno)
perror("Error");
printf("The arc hyperbolic sine of %f is %f\n", x, y);
errno = 0;
x = 1.0;
y = asinh(x);
if (errno)
perror("Error");
printf("The arc hyperbolic sine of %f is %f\n", x, y);
errno = 0;
x = 720.0;
y = asinh(x);
if (errno)
perror("Error");
printf("The arc hyperbolic sine of %f is %f\n", x, y);
}
Example Output
The arc hyperbolic sine of -1.000000 is -0.881374
The arc hyperbolic sine of 1.000000 is 0.881374
The arc hyperbolic sine of 720.000000 is 7.272399