Converts a multibyte character to a wide character.
Include
<stdlib.h>
Prototype
int mbtowc(wchar_t * restrict pwc, const char * restrict s, size_t
n);
Arguments
pwc | |
s | |
n |
Return Value
If s
is a null pointer, the function returns a nonzero or zero value, which
indicates if multibyte character encodings, respectively, do or do not have state-dependent
encodings.
If s
is not a null pointer, the function returns 0 if s
points to the null character, returns −1 if the processed bytes do not form a valid multibyte
character, or returns the number of bytes of the converted multibyte character.
The returned value will never exceed n
or the value of the
MB_CUR_MAX
macro.
Remarks
If a valid multibyte character (including any shift sequences) can be formed from no more
than the next n
bytes of the sequence pointed to by s
, that
multibyte character is converted to a wide character that is then stored to the object pointed
to by pwc
, provided that pointer is not null. If the corresponding wide
character is the null wide character, the function is left in the initial conversion
state.
Example
See the notes at the beginning of this chapter or section for
information on using printf()
or scanf()
(and other functions reading and writing the stdin
or
stdout
streams) in the example code.
#include <locale.h>
#include <wchar.h>
#include <stdlib.h>
void printWide(const char * mbstr)
{
size_t len;
wchar_t wstr;
mbtowc(NULL, 0, 0); // reset the conversion state
while(*mbstr) {
len = mbtowc(&wstr, mbstr, 40);
wprintf(L"%lc(%d)", wstr, len);
mbstr += len;
}
wprintf(L"\n");
}
int main(void)
{
setlocale(LC_CTYPE, "");
printWide("PIC®");
}
Example Output
P(1)I(1)C(1)®(2)