Convert wide string to a long double precision floating-point value.
Include
<wchar.h>
Prototype
long double wcstold(const wchar_t * restrict nptr, wchar_t ** restrict
endptr);
Arguments
nptr | |
endptr |
Return Value
The converted value, or 0 if the conversion could not be performed. If the correct value of
the conversion is outside the range of representable values, HUGE_VAL
is
returned with a sign being that of the correct value. If the result underflows, the function
returns a value whose magnitude is no greater than the smallest normalized positive number in
the return type.
Remarks
The wcstold
function attempts to convert a portion of the wide string
pointed to by nptr
to a long double
floating-point
value.
The initial section consists of any white-space wide characters.
e
or E
followed by an option sign
and decimal digits0x
or
0X
, then a nonempty sequence of hexadecimal digits
optionally containing a decimal-point wide character, then an optional
binary exponent part, being p
or P
, and
option sign, and decimal digits.INF
or INFINITY
, ignoring caseNAN
,
ignoring case, optionally followed by any sequence contain digits or
non-digits:endptr
, provided that
endptr
is not a null pointer.The final section consists of wide characters in the wide string that were
unrecognized in the subject section and which will include the terminating null wide
character of the wide string. This section of the wide string will be accessible via
the address stored to endptr
, provided endptr
is
not a null pointer.
The value of the macro ERANGE
is stored in errno
if
the correct value of the conversion is outside the range of representable values.
The errno
variable is not set to ERANGE
if the
result underflows.
Example
#include <wchar.h>
int main(void)
{
wchar_t ws[] = L"2000.5 -6.0E-3 0x70FF INFINITY";
wchar_t * pEnd;
long double d1, d2, d3, d4;
d1 = wcstold(ws, &pEnd);
d2 = wcstold(pEnd, &pEnd);
d3 = wcstold(pEnd, &pEnd);
d4 = wcstold(pEnd, NULL);
wprintf(L"The converted string values are: %Lg, %Lg, %Lg, and %Lg.\n", d1, d2, d3, d4);
}
Example Output
The converted string values are: 2000.5, -0.006, 28927, and inf.