Gets the current rounding direction.
Include
<fenv.h>
Prototype
int fegetround(void);
Return Value
This function returns the a value representing the current floating-point rounding direction, which can be compared to the rounding-direction macros.
Example
See the notes at the beginning of this chapter or section for
information on using printf()
or scanf()
(and other functions reading and writing the stdin
or
stdout
streams) in the example code.
#include <fenv.h>
#include <stdio.h>
#include <assert.h>
int main(void)
{
int save_round, setround_ok;
volatile double x, y=1E30;
save_round = fegetround(); // save the rounding state
setround_ok = fesetround(FE_UPWARD);
assert(setround_ok == 0);
x = 1 / y;
printf("the small result rounded up is %.40f\n", x);
setround_ok = fesetround(FE_DOWNWARD);
assert(setround_ok == 0);
x = 1 / y;
printf("the small result rounded down is %.40f\n", x);
fesetround(save_round); // restore the rounding state
}
Example Output
the small result rounded up is 0.0000000000000000000000000000010000000001
the small result rounded down is 0.0000000000000000000000000000009999999999