Calculates the trigonometric tangent function of a long double precision floating-point value.
Include
<math.h>
Prototype
long double tanl(long double x);
Argument
x |
Return Value
Returns the tangent of x
specified in radians in the range
x
is
Example
See the notes at the beginning of this chapter or section for
information on using printf()
or scanf()
(and other functions reading and writing the stdin
or
stdout
streams) in the example code.
#include <math.h>
#include <stdio.h>
#include <errno.h>
int main(void)
{
long double x, y;
errno = 0;
x = -1.0;
y = tanl(x);
if (errno)
perror("Error");
printf("The tangent of %Lf is %Lf\n", x, y);
errno = 0;
x = 0.0;
y = tanl(x);
if (errno)
perror("Error");
printf("The tangent of %Lf is %Lf\n", x, y);
}
Example Output
The tangent of -1.000000 is -1.557408
The tangent of 0.000000 is 0.000000