Calculates the complex cosine function of a double precision complex value.
Include
<complex.h>
Prototype
double complex ccos(double complex z);
Argument
z |
Return Value
Returns the complex cosine of z
.
Example
See the notes at the beginning of this chapter or section for
information on using printf()
or scanf()
(and other functions reading and writing the stdin
or
stdout
streams) in the example code.
#include <stdio.h>
#include <complex.h>
int main(void)
{
double complex x, y;
x = -2.0 + 1.0*I;
y = ccos(x);
printf("The complex cosine of %f + %fi is %f + %fi\n", creal(x), cimag(x), creal(y), cimag(y));
}
Example Output
The complex cosine of -2.000000 + 1.000000i is -0.642148 + 1.068607i