Determine accessibility of a file
Include
<unistd.h>
Prototype
int access(const char * filename, int how);
Arguments
filename | |
how |
Return Value
The return value is 0 if the access is permitted, and -1 otherwise. For the value -1,
errno
is set to indicate the kind of error. Appropriate values may
be EACCES
, ENOENT
or EROFS
, among
others.
Remarks
This function is implemented as a stub that must be completed to suite the application.
The access
function checks to see whether the file named by
filename
can be accessed in the way specified by the
how
argument. The argument either can be the bitwise OR of the
flags R_OK
, W_OK
, X_OK
, or the
existence test F_OK
This function uses the real user and group IDs of the calling process, rather than
the effective IDs, to check for access permission. As a result, if you use the
function from a setuid
or setgid
program, it gives
information relative to the user who actually ran the program.
Source File
access.c