In Timer Adjust mode, the tsu_clk is supplied from the FPGA fabric. The maximum clock frequency is 125 MHz. There are several signals, synchronous to tsu_clk output by the MAC.
In this mode, the timer operation is also controlled from the fabric by input signals called gem_tsu_inc_ctrl [1:0] along with gem_tsu_ms.
When the gem_tsu_inc_ctrl [1:0] is set to:
The TSU timer count value can be compared to a programmable comparison value. For the comparison, the 48 bits of the seconds value and the upper 22 bits of the nanoseconds value are used. The timer_cmp_val signal is output from the core to indicate when the TSU timer value is equal to the comparison value stored in the timer comparison value registers.
The following diagram shows TSU from fabric in Timer Adjust mode.