0 |
No error |
— |
1 |
Bitstream authentication failed |
Invalid bitstream or wrong key used. |
2 |
Unexpected data received |
Additional data is received after end of bitstream component. |
3 |
Invalid/corrupt encryption key |
The requested key mode is disabled or the key could not be read/reconstructed. |
4 |
Invalid component header |
Invalid bitstream |
5 |
Back level not satisfied |
Bitstream version is older than that of the current back level value set in the device. |
6 |
Illegal bitstream key mode |
Bitstream key mode is not initialized or bitstream key mode is disabled by user security. |
7 |
DSN binding mismatch |
Bitstream is rejected because DSN in the bitstream does not match with the DSN present in the device. A bitstream can be bound to device's unique DSN such that only a specific device can be programmed with that bitstream. |
8 |
Illegal component sequence |
Incorrect bitstream |
9 |
Insufficient device capabilities |
Bitstream is rejected because the capabilities specified in the bitstream do not match the target device's capabilities. |
10 |
Incorrect DEVICEID |
Bitstream is rejected because an attempt by the DEVICEID specified in the bitstream does not match the part identification field (for example, MPF300, MPF500 and so on) of the target device. |
11 |
Unsupported bitstream protocol version (bitstream regeneration required) |
Bitstream is rejected because of an attempt made by the old version of a device to decode a bitstream created in new format or by the new version of a device to decode a bitstream created in old format. |
12 |
Verify not permitted on this bitstream |
Verify programming action is disabled in the bitstream. |
13 |
Invalid Device Certificate |
Device certificate is invalid or not present. |
14 |
Invalid DIB |
Device integrity bits (DIB) are invalid. |
21 |
Device not in SPI Master Mode |
Error may occur only when bitstream is executed through IAP mode. The System Controller SPI controller is not configured in master mode. |
22 |
No valid images found |
Error may occur when bitstream is executed through Auto Update mode. Occurs when No valid image pointers are found. |
23 |
No valid images found |
Error may occur when bitstream is executed through IAP mode via Index Mode. Occurs when No valid image pointers are found. |
24 |
Programmed design version is the same as the Auto Update image found |
Error may occur when bitstream is executed through Auto Update mode. |
25 |
Reserved |
Reserved
|
26 |
Selected image was invalid and no recovery was performed due to valid design in device. |
Error may occur only when bitstream is executed through Auto Update or IAP mode. Error could also occur due to BACKLEVEL protection. |
27 |
Selected and Recovery image failed to program |
Error may occur only when bitstream is executed through Auto Update or IAP mode. |
127 |
Abort |
Non-bitstream instruction is executed during bitstream loading. |
128 |
NVMVERIFY |
Fabric or security segment verification failed. |
129 |
PROTECTED |
Device security is prevented modification of non-volatile memory. |
130 |
NOTENA |
Programming mode not enabled |
131 |
PNVMVERIFY |
pNVM verify operation failed |
132 |
SYSTEM |
System hardware error (PUF or DRBG) |
133 |
BADCOMPONENT |
An internal error was detected in a bitstream component payload. |
134 |
HVPROGERR |
Failure in programming subsystem. |
135 |
HVSTATE |
Error in the programming subsystem. |