This user interface provides framework to add firmware files that enables usage of push-button. The push-button needs to be connected to the GPIO pin as shown in the image below. The UI provides options for the GPIO pin input configuration drive - Internal Pull Up, Internal Pull Down and None.
The option 'None' means that neither Internal pull-up nor Internal pull-down is used and the pull-up or pull-down resistor will be available external to the microcontroller.
Click on the checkbox near the 'Push Button' module on the panel on the left hand side to enable this module to be added to the project
Select a GPIO pin and input mode
Currently only one push-button can be configured and added to the project.