This page lists a set of firmware code modules that can be optionally added to the project. This creates a framework that can be enhanced further by adding application logic. The following are the supported firmware modules:
Category | Name of the module |
---|---|
Debugging | USART serial communication |
Periodic Operations | Periodic Operations Using Timer |
Low Power Sleep And Wake mechanism | |
Transceiver Feature Access | Transceiver Features |
User Interface | LED |
Push Button |
Click on the button Next to view Summary Page.