AVR2025 MAC stack supports SW-implemented Timers that can be utilized by the wireless applications. The timer has a resolution of 1μs. Selecting this module provides framework to configure the SW timer.
Click on the checkbox near the 'Using Timer' module on the panel on the left hand side to enable this module to be added to the project
Select a time duration for the periodic operation. (The validation is done to ensure that the time duration entered is within the acceptable range.)