This user interface provides framework to add firmware files that will contain APIs to drive a LED. The LED and a series resistor needs to be connected to the GPIO pin as shown in the image below. The UI provides two options for the GPIO pin output drive - Active Low and Active High.
Click on the checkbox near the 'LED' module on the panel on the left hand side to enable this module to be added to the project
Select a GPIO pin and drive mode
Currently only one LED can be configured and added to the project.