This module provides framework to configure a USART port to enable debugging and communication with other systems.
Click on the checkbox near the Usart Serial module on the panel on the left hand side to enable this module to be added to the project
Select USART module (e.g., USARTC0, USARTC1, or USART01)
Configure the following parameters; Data bits length, Baud rate, Parity, and No of stop bits
Assign RX and TX pins
Ensure that the pins used for USART is not used in any other parts of the wizard