The synchronization is done only in slave node configuration. The procedure is based on time measurement between falling edges of the Synch Field. The falling edges are available in distances of 2, 4, 6 and 8 bit times.
The time measurement is made by a 19-bit counter clocked by the sampling clock (see “Baud Rate Generator”).
When the start bit of the Synch Field is detected, the counter is reset. Then during the next eight tbit of the Synch Field, the counter is incremented. At the end of these eight tbit, the counter is stopped. At this moment, the 16 most significant bits of the counter (value divided by 8) give the new clock divider (LINCD) and the three least significant bits of this value (the remainder) give the new fractional part (LINFP).
Once the Synch Field has been entirely received, the clock divider (LINCD) and the fractional part (LINFP) are updated in the LIN Baud Rate register (US_LINBRR) with the computed values, if the Synchronization is not disabled by the SYNCDIS bit in the LIN Mode register (US_LINMR).
After reception of the Synch Field:
Flags LINSTE and LINISFE are reset by writing US_CR.RSTSTA to ‘1’.
The accuracy of the synchronization depends on several parameters:
The following formula is used to compute the deviation of the slave bit rate relative to the master bit rate after synchronization (fSLAVE is the real slave node clock frequency):
fTOL_UNSYNCH is the deviation of the real slave node clock from the nominal clock frequency. The LIN Standard imposes that it must not exceed ±15%. The LIN Standard imposes also that for communication between two nodes, their bit rate must not differ by more than ±2%. This means that the baud rate deviation must not exceed ±1%.
It follows from that, a minimum value for the nominal clock frequency:
Examples: