The Xmodem protocol supported is the 128-byte length block. This protocol uses a two-character CRC-16 to guarantee detection of a maximum bit error.
The Xmodem protocol with CRC is accurate if both sender and receiver report successful transmission. Each block of the transfer has the following format:
<SOH><blk #><255-blk #><--128 data bytes--><checksum> in which:
The figure below shows a transmission using this protocol.