The scanner module may be used in conjunction with the CRC module to perform a CRC
calculation over a range of program memory or Data EEPROM addresses. To set up the
scanner to work with the CRC, perform the following steps:
- 1.Set up the CRC module (see the
“Configuring the CRC Module” section) and enable the scanner module
by setting the EN bit in the SCANCON0 register.
- 2.Choose the scanning mode by
configuring the MD bits.
- 3.If Trigger mode is selected for
scanner operation, select the trigger source using the TSEL bits.
- 4.Set the SCANLADR and SCANHADR registers with the beginning and ending
locations in memory that are to be scanned.
- 5.Both EN and GO bits in the CRCCON0 register must be enabled to use the scanner. Setting the
SGO bit will start the scanner operation.