The ZCD module can be disabled in two
ways:
- 1.The ZCD
Configuration bit disables the ZCD module when set. When this is the case, then the ZCD
module will be enabled by setting the SEN bit.
When the ZCD bit is clear, the ZCD is
always enabled and the SEN bit has no effect.
- 2.The ZCD can also be disabled using the ZCDMD bit of the PMDx
register. This is subject to the status of the ZCD bit.