Define stimulus triggers in each row of this section as shown in the table below, with reference to the conditions set up in “Define Conditions”.
Item | Definition |
---|---|
Enable | Alternately enable or disable the trigger setup in this row. |
Condition | Refers to the label of the condition set up in the “Define Conditions” section of this tab. Select a condition from the list. |
Type | Select whether the trigger condition will apply once (1x) or continuously/ repeatedly (Cont). |
Re-Arm Delay | If Type = Cont, then enter a delay until the trigger condition is checked again. The delay value is entered in the first column and the delay value unit is selected in the second column. |
Click here to Add Signals | Click on the column title to open the Add/Remove Pin/Registers Dialog. In this dialog, you select the pins, registers or other signals to which you will apply stimulus. These selections will become the titles of the columns. |
To scroll through signals:
For the condition set up in Define Conditions, COND1, set up the following stimulus trigger: