Check and verify all the pin names in the design. To verify the pin names, double-click I/O Constraints in the Design Flow tab as shown in the following figure.
The I/O Editor dialog lists the port names with the updated pin names as shown in the following figure. The pin names that are not modified follow the Microchip pin naming convention.
For the I/O Editor dialog to open, the design must be synthesized and compiled.
To export the pin names, double-click Export Pin Report in
the Design Flow tab. This report has the file extension
.rpt
.
The report is stored in the project directory. The path is: <Libero Project Directory>\designer\project\export\<project Name>_top_pinrpt_number.rpt.