For concise equations, we’ll use the following notations:
Using the (tempR, ADCR) and (tempH, ADCH) points, using a linear interpolation we have the following equation:
Given a temperature sensor ADC conversion value ADCm, we can infer a coarse value of the temperature tempC as:
[Equation 1]
Note 1: in the previous expression, we’ve added the conversion of the ADC register value to be expressed in V
Note 2: this is a coarse value because we assume INT1V=1V for this ADC conversion.
Using the (tempR, INT1VR) and (tempH, INT1VH) points, using a linear interpolation we have the following equation:
Then using the coarse temperature value, we can infer a closer to reality INT1V value during the ADC conversion as:
Back to [Equation 1], we replace INT1V=1V by INT1V = INT1Vm, we can then deduce a finer temperature value as:
[Equation 1bis]