The temperature sensor behavior is linear but it depends on several parameters such as the internal voltage reference which itself depends on the temperature. To take this into account, each device contains a Temperature Log row with data measured and written during the production tests. These calibration values should be read by software to infer the most accurate temperature readings possible.
This Software Temperature Log row can be read at address 0x00806030. The Software Temperature Log row cannot be written.
This section specifies the Temperature Log row content and explains how to refine the temperature sensor output using the values in the Temperature Log row.