Design objects such as port, nets, and instances can be added to a logical cone.
- When a net is selected and added to the cone, the
instance connected to the net is added, and the net is a solid line in the
cone.
- Nets that are automatically added to the view (because of added instances) will
always be shown as dashed (regardless of whether or not they have additional
connections not yet added to the view).
- Nets are solid lines when they are
added through the tree, or double-clicking a dashed net, or when adding a port to
the view, which adds its attached net.
- Ports are not added to the view if an attached dashed net is already in the
view.
- When an instance is selected and added to the cone, all the partial nets of the
instance are added to the instance pins. Nets which are represented by dash lines
are partial nets, which are automatically added to the cone view when an instances
is added. Double-clicking a partial net in a cone view adds to the cone all the
ports and instances the partial net is connected to. The dashed net changes to a
solid line.
To add design objects to a logical cone:
- 1.Make sure the cone to which you
want to add design objects is the Target Cone. Only one cone can be active at a
time.
- 2.In Netlist Viewer or a Logical
Cone view, select the instance, pin, or net to add to the logical cone.
- 3.From the Netlist Viewer/Logical
Cone view, choose Add to Target Cone > Selection.
Note: When an instance is added to a logical cones, all the lower levels of hierarchy, if
any, of the instance are included in the logical cone. The instance in the cone can be
expanded in place (by clicking the “+” sign) or folded/collapsed (by clicking the “-”
sign).
Figure 1. Adding Design Objects to Active Logical Cone