Use one of the following two ways to execute the Expand Inplace operation
on an instance.
- Click the + button at the
top left of the instance, which indicates that it is pushable.
Figure 1. Expand in Place icon
- Left-click to select the instance and then
right-click to select Expand Inplace.
Figure 2. Expand Inplace Menu Selection