When reprogramming is initiated, the FPGA is erased. Therefore, the programming and stand-alone verify operations must be completed to success, otherwise the FPGA will be inoperable. The following sequence must be followed when performing in-flight reprogramming:
For information about timing requirements and interface to the RT PolarFire FPGA JTAG pins, see JTAG Programming.
The following figure shows the sequence of in-flight reprogramming.