The following figure illustrates the Polling Configuration within the Polling tab for setting up the polling operation of the ATA8510 device. For more details about the EEPROM polling configuration, refer to the ATA8510/15 Industrial User's Guide (DS50003142).
For more details about the default settings for the Polling tab, refer to Default Configuration.
The default Polling Configuration is subdivided into three polling cycle definitions with alternating channel scanning order for Service 2. In addition, enable the VCO tuning for PollConf 0, set the “Target Polling Cycle” to 50 ms, and set the Timer Clock Source to SRC.