The following sections provide details about the EEPROM configuration and further information about the settings in the configuration tabs of the EEPROM configuration tool. The EEPROM configuration tool includes the following tabs:
The values and settings in the following figures represent the default configuration. After
launching the EEPROM configuration tool, the ATA5831_EEPROM_default.xml
file loads the default configuration. For more details, refer to the ATA8510/15
Industrial User's Guide (DS50003142).