Erases the Secondary core to the erase state.
Include
<libpic30.h>
Prototype
int _wipe_secondary(int secondary_number)
Arguments
secondary_number
|
Identifier of the Secondary core to be
programmed. The identifier for the first Secondary core is
1 . |
Return Value
Remarks
None.
Default Behaviour
The _wipe_secondary
routine can be used to completely wipe the PRAM
memory of the Secondary core. This routine will always wipe the entire memory range,
even if dual partition mode is selected.
File
wipe_secondary.c
(in
libpic30.zip>data_init_dualch.S
)