Copies bytes from one __eds__
buffer to another __eds__
buffer.
Include
<libpic30.h>
Prototype
__eds__ void* _memcpy_eds(__eds__ void *dest, __eds__ void
*src, unsigned int len);
Arguments
dest |
destination memory address |
src |
address of data to be written |
len |
length of program memory |
Return Value
The memory block pointed to by dest
.
Remarks
__eds__
pointers are superset of unqualified data pointers; therefore
these functions can be used to copy between __eds__
and unqualified
data memory.
Default Behavior
Copy len
bytes of data from each address pointed to by the
src
pointer to the destination pointed to by the
dest
pointer.
File
memcpy_helper.s