Copies bytes from one __pack_upper_byte
Flash buffer to
another buffer in RAM.
Include
<libpic30.h>
Prototype
void* _memcpy_packed(void *dest, __pack_upper_byte void
*src, unsigned int len);
Arguments
dest |
destination memory address |
src |
address of data to be written |
len |
length of program memory |
Return Value
The memory block pointed to by dest
.
Remarks
None.
Default Behavior
Copy len
bytes of data from each address pointed to by the
src
pointer to the destination pointed to by the
dest
pointer.
File
memcpy_helper.s