Copies a string from one __pack_upper_byte
Flash buffer to
another buffer in RAM.
Include
<libpic30.h>
Prototype
void* _strcpy_packed( void *dest, __pack_upper_byte void
*src);
Arguments
dest |
destination memory address |
src |
address of data to be written |
Return Value
The string pointed to by dest
.
Remarks
None.
Default Behavior
Copy the string pointed to by src
to the RAM buffer pointed
to by dest
. Unlike the standard strncpy
function, this
function does not zero fill the remaining space in the destination string.
File
memcpy_helper.s