Programs the inactive partition PRAM with the specified image.
Include
<libpic30.h>
Prototype
int _program_inactive_secondary(int secondary_number, int verify,
__eds__ unsigned char *image)
Arguments
secondary_number
|
Identifier of the Secondary core to be
programmed. The identifier for the first Secondary core is
1 . |
verify
|
A 0 will load the entire
Secondary image to the PRAM. A 1 will verify the entire
image in the PRAM. |
*image |
Pointer to the image to be programmed into
PRAM. Secondary PRAM images not following the Microchip language tool format will require a custom routine. |
Return Value
Remarks
The Main core loads the PRAM inactive partition while the Secondary core is running and
then the Secondary core executes the BOOTSWP
instruction to swap
partitions.
Default Behavior
The _program_inactive_secondary
routine uses the
verify
parameter as a switch to either load or verify the
inactive partition image using the LDSEC
or VFSEC
instructions.
File
program_inactive_secondary.c
(in
libpic30.zip>data_init_dualch.S
)