The Dimmable Light application is part of the ZigBee Light Link (ZLL) reference application in the BitCloud SDK.
The Figure 1 shows the BitCloud SDK package. The Dimmable Light
application files are present in the \Light
inside the \Applications\ZLLDemo
folder.
\BitCloud\lib
contains the BitCloud core stack library and
hardware abstraction layer(HAL) libraries to be built along with the application.The Figure 3 is also provided in the firmware package available with the application note.
Note: The firmware is based on BitCloud SDK version 3.2.0 and the IAR™ and Atmel Studio versions are as per the BitCloud Quick Start Guide.