AT13519
Dimmable Light – The ATSAMR21-LED-Driver Board
The firmware for the ATSAMR21-LED-Driver Board is an integration of two major components:
1.
The LED driver for driving the LED load.
2.
The ZigBee BitCloud SDK for wireless control of the light.
Source Code Organization
Project Configuration
Configuration of Parameters
Memory Footprint
Operating Principles of the LED Driver
ZigBee Functionalities of the Dimmable Light