A Flash/EEPROM write or erase can cause memory corruption if the supply voltage is too low
for the CPU and the Flash/EEPROM to operate correctly. These issues are the same on-board
level systems using Flash/EEPROM, and it is recommended to use the internal or an external
Brown-out Detector (BOD) to ensure that the operating voltage is high enough.
Two circumstances may cause Flash/EEPROM corruption when the voltage is too low:
- 1.A regular write sequence to the
Flash, requiring a minimum voltage to operate correctly.
- 2.The CPU itself can execute
instructions incorrectly when the supply voltage is too low.
The chip erase does not clear fuses. If the BOD is enabled by fuses before starting the
Chip Erase command, it is automatically enabled at its previous configured level during the
chip erase.
Refer to the Electrical Characteristics section for Maximum Frequency
vs. VDD.
Attention: Taking the following
measures may avoid Flash/EEPROM corruption:
- 1.Keep the device in Reset during
periods of insufficient power supply voltage. Do this by enabling the internal
BOD.
- 2.The Voltage Level Monitor (VLM) in
the BOD can be used to prevent starting a write to the EEPROM close to the BOD
level.
- 3.If the detection levels of the
internal BOD do not match the required detection level, an external VDD
Reset protection circuit can be used. If a Reset occurs while a write operation is
ongoing, the write operation will be aborted.