Sanity Check
Possible Reason
Marginal issues on CA, Write DQ/DQS, or Read DQ/DQS. When the Sanity Check fails, a dialog box appears as shown in the following figure.
Figure 1.
Sanity Check
Workaround
Configure any one of the following parameters to a different value using the MSS Configurator when the Sanity Check fails:
Memory CA ODT
FPGA DQ Drive
FPGA DQS Drive
FPGA DQ ODT
FPGA DQS ODT
Memory Pull-Down Drive Strength
The following figure shows the configuration of DQ/DQS drive or ODT in the
DDR Controller
tab.
Figure 1.
Configuring DQ/DQS Drive or ODT—DDR Controller Tab
The following figure shows the configuration of pull-down drive strength or CA ODT in the
DDR Memory Initialization
tab.
Figure 2.
Configuring Pull-Down Drive Strength or CA ODT—DDR Memory Initialization Tab
Parent topic:
Troubleshooting