The following steps describe how to setup the hardware:
- 1.Power OFF the board using the SW7 switch.
- 2.Retain the default setting for J31 jumper to use
the external FlashPro programmer.
- 3.Connect the host PC to the J24 connector using
the USB cable.
- 4.Connect the FlashPro programmer to J3 connector
(JTAG header) and use another USB cable to connect the FlashPro programmer to the
Host PC.
- 5.Ensure that the USB to UART bridge drivers are
automatically detected. Verify it in the device manager of the host PC.
- 6.Connect the power supply to J19
connector and switch ON the power supply switch SW7.