To remove all the synthesis attributes from the object, right click the SD module and SD objects (port, net, and instance), and click Clear Synthesis Attributes as shown in the following figure.
You can use Manage Synthesis attributes toolbar to open Manage Synthesis Attributes window as shown in the following figure. This window allows users to add or modify attributes of the SmartDesign objects.
After selecting an object (port, net, and instances) in the SmartDesign canvas, the attributes of the selected object are displayed in the Manage Synthesis Attributes window. The Manage Synthesis Attributes window displays the SmartDesign module attributes if no object is selected. The name of the selected object is displayed on the window.
All the attributes, reflected in the drop-down menu, are intended for the selected object. As the user selects the attribute from the drop-down list, the attribute is automatically added with a default value. To change the default value of the attribute, double click the value field. The selected attribute description is displayed at the bottom of the window.
The tool-tip shows the vendor and technology of the attribute. To remove one or more attributes, select them and click Manage Synthesis Attributes the Manage Synthesis Attributes window Toolbar. To delete all the attributes of the selected object, click Remove all Synthesis attributes on the Manage Synthesis Attributes window Toolbar.