This section details the hardware requirements for running the various BM70/71 ASF demo
applications.
The following are the instructions for the hardware setup to work as a GAP-Central and
GAP-Peripheral device according to the application requirement.
- 1.Plug the BM70/71-Xpro into the
EXT1 header of SAML21 Xplained Pro as illustrated in the following figure.
Note: Step 1 is common for both the
GAP-Central and GAP-Peripheral device.
- 2.For the GAP-Peripheral device,
plug in the BNO055 board into the EXT2 of SAML21 Xplained Pro as illustrated in
the following figure.
Figure 1. GAP-Central
Device Hardware Setup
Figure 2. GAP-Peripheral Device Hardware Setup
- 3.Connect the SAML21 Xplained Pro
board to the host PC using a micro USB cable. The following table provides the
application-based hardware requirements necessary for running various BM70/71
ASF demo applications.
Application |
GAP-Central Device |
GAP-Peripheral Device |
MBD Mobile Application |
GAP-Central Demo |
Yes |
Yes |
No |
GAP-Peripheral Demo |
Yes |
Yes |
Yes |
iBeacon Demo |
Yes |
No |
Yes |
Multilink Central |
Yes |
Yes |
No |
Multilink Multirole |
Yes |
Yes |
Yes |
Transparent UART Demo |
Yes |
No |
Yes |