Programming the Target Using an External Programmer

How to program the target ATmega168PB using the AVR® JTAGICE mkII, JTAGICE3, Atmel-ICE, or other programmers.

  1. 1.Connect the External Programmer USB to the PC.
  2. 2.Connect the External Programmer to the ATmega168PB Xplained Mini board ISP connector.
  3. 3.Go to Atmel Studio: Click the Tools tab, select Device Programming, and select the External Programmer connected as Tool with Device as ATmega168PB and Interface to ISP, click Apply.
  4. 4.Select “Memories”, locate the source .hex or .elf file, and click Program.