User LED

There is one yellow LED, D200, available for use by the application SW.

The LED is connected to ATmega168PB pin 17 - PB5, the SCK signal from the mEDBG is in 3-state when not used.

Figure 1. User LED