The manifest files only contain public information of the device, such as its serial number, certificates and slots’ public information. Depending on the configuration differences, the information in Trust&GO, TrustFLEX and TrustCUSTOM files varies as follows:
Trust&GO | TrustFLEX | TrustCUSTOM |
---|---|---|
|
|
|
When the user opts to create a custom certificate chain on the TrustFLEX device, the factory provisioned certificates will be overwritten. Trust Platform Design Suite scripts/notebook allow the user to back up default certificates into a local folder before overwriting custom certificates on the device. However, if the board changes hands after provisioning, the new user will not have the back-up certificates and will not be able to revert to factory default.